Configure the OPC server

You configure an OPC server to ensure it is connected and its status is regularly communicated to your OPC client.

Before you begin

Add an OPC client.

Procedure

  1. In the navigator, click Proficy System > Proficy System > OpcClient.
  2. From the OPC Servers list, select the OPC server you want to configure.
  3. From the Displays panel, select HW/SW > Data Source Editor.
    The Data Source Editor appears.
  4. If applicable, select a new server Prog ID:
    1. Click the ellipsis button next to the Server Prog ID field.
      The Select OPC Server Prog ID dialog box appears.
    2. Select the Prog ID of the OPC server you want to connect to, and then click OK.
  5. In the Health Monitor Frequency field, enter how often, in milliseconds, the OPC server communicates its health status to the OPC client.
    Note:
    • If you are using OPC DA v2.0x, the client communicates with the server at this interval to monitor the health status.
    • If you are using OPC DA v3.0, the server communicates with the client at this interval to monitor the health status.
  6. Click Refresh.
    The OPC server status information is displayed.
    Note:
    The OPC server status information is not automatically refreshed; you must refresh the status manually.
  7. Click Save.