Add an OPC client

You connect your OPC client to an OPC server that is installed on your application server computer.

Procedure

  1. In the navigator, click Proficy System > Proficy System > OpcClient.
  2. Click Add OpcServer.
  3. In the Name field, enter a name for the OPC server you want to connect to.
  4. Optionally, in the Description field, enter a description of the OPC server.
  5. In the Server Prog ID field, enter the Prog ID of the OPC server you want to connect to.
    - Or -

    Click the ellipsis button to open the Select OPC Server Prog ID dialog box where you can select the OPC server you want to connect to.

    Refer to your OPC server documentation to determine the Prog ID.

  6. Click OK.