Add a GE Historian server

You can add an GE Historian server as a data source.

Before you begin

Note:
Workflow supports GE Historian 4.5 or greater.

Procedure

  1. In the navigator, click Proficy System > Proficy System > Historian.
  2. Click Add Historian.
  3. In the Display Name field, enter either the actual name of the GE Historian server you want to connect to or an alias for the server name.
    The name you enter in this field is automatically entered into the Server Name field.
  4. If you entered an alias in the Display Name field, then in the Server Name field, enter the GE Historian server address.
    Note:
    The GE Historian server address must comply with a valid Windows® computer name; however, the underscore character is permitted.
  5. Optional: Enter a description of the GE Historian server.
  6. If security is enabled on the GE Historian server, enter the user name, password, and domain for this server.
  7. Click OK.