WriteSegmentParameters (IProductionModel)
Writes to the parameters of a specified work definition segment.
Note:
- This write modifies configuration data of the work definition segment, as well as all work requests that are subsequently created against any work definitions that contain the segment.
- In the Configure Method dialog box, click Next to select a work process segment whose parameters you want to write to. The parameters appear in the Inputs area of the activity configuration panel.
Inputs | Data Type | Description |
---|---|---|
Work Definition Segment input parameters | Dependent on each parameter's data type | Specifies the values for the parameters to write. |
Work Definition Segment | DirectoryResource |
Specifies a work definition segment that associated with the work process segment that contains the parameters you want to write to. |