AddMasterSegmentToWorkDefinition (IProductionModel)
Adds a master segment to a work definition.
A master segment is a work process segment that contains information that applies to all work definition segments associated with a work definition. In other words, a master segment is a template for a work request. For example, a customer name can be represented as a segment parameter in a master segment.
A master segment can be associated with multiple work definitions; however, a work definition can be associated with only one master segment. Work requests are created from an individual work definition and, therefore, can also be associated with only one master segment.
Inputs | Data Type | Description |
---|---|---|
Master Segment | DirectoryResource |
Specifies the work process segment to add to the selected work definition as the master segment. |
Work Definition | DirectoryResource | Specifies the work definition to add the master segment to. |