StartResourceLink (IResourceLinking)

Starts a user-defined resource link between two resources.

InputsData TypeDescription
Resource Link NameStringSpecifies a name for the resource link.
Note:
You can create multiple resource links with the same name; however, the source and/or target resources must be unique for each resource link.
Source AddressDirectoryResourceSpecifies the source resource for the resource link.
Start TimeDateTime(Optional) Specifies the start date and time for the resource link.
Note:
If the Start Time field is blank, the start time defaults to the current date and time when the call method runs.
Target AddressDirectoryResourceSpecifies the target resource for the resource link.

OutputsDescription
GUID The unique ID of the new resource link.