AlterResourceLink (IResourceLinking)

Modifies an existing user-defined resource link.

InputsData TypeDescription
End TimeSateTime(Optional) Specifies a new end time for the link. If you leave this field blank, then the resource link's end time does not change.
Note:
If the resource link already has an end time defined, you can modify it to an earlier or later date and/or time. If the resource link does not have a defined end time, you can set it here. In either case, the end time must be later than the start time.
Resource Link IDGUIDSpecifies the unique ID of the resource link you want to work with.
Resource Link NameString(Optional) Specifies the new name for the resource link. If this field is blank, then the resource link name does not change.
Start TimeDateTime(Optional) Specifies the new start time for the resource link. If you leave this field is blank, then the resource link's start time does not change.
Note:
In the Configure Method dialog box, click Next to select a resource. Otherwise, in the Inputs section of the activity configuration panel, click the ellipsis button to select a resource.