Viewing Session Information

About this task

The Webspace Admin Console displays the following session information: Session Name, User Name, Connected Clients, IP Address, Startup Time, and Applications. You can find this information on the Sessions tab.

Procedure

  1. To view session information, click the Sessions tab.
  2. See the following table for a description of each field.
    Column Description
    Session Name

    Unique identifier assigned to each session.

    User

    Network user name of the user accessing the server.

    Connected Clients

    The number of clients connected to a session. 0 indicates that no one is connected to the session (the client has disconnected). 1 indicates that the client is connected, and the session is active. 2 or higher indicates that the session is being shadowed.

    IP Address IP address of the client computer from which the user is accessing the server. (Each computer on a network has a unique IP address.)
    Startup Time

    Date and time the user started the application.

    Applications

    Number of processes the user is accessing.