Refreshing the Webspace Admin Console
About this task
You can update the information displayed in the Webspace Admin Console manually or you can set it to update automatically. If the Webspace Admin Console is set to update automatically, you can still update it manually at any time.
For information about setting the Webspace Admin Console to update automatically or manually, refer to the Setting the Refresh Rate in the Webspace Admin Console section.
Procedure
- From the Webspace Admin Console, on the server list, select the desired server.
- On the View menu, click Refresh. The data should refresh in the window as you are viewing it.