Restarting the Proficy Webspace Application Publishing Service

About this task

There may be times when you need to restart the Proficy Webspace Application Publishing Service. For example, if you change the SCU path on the Applications tab, after you already entered it for the first time, you will need to restart this service.

You can restart the service from the Webspace group on the Start menu, or from the Services window from the Windows Administrative tools.

Procedure

  1. On the Start menu, point to Programs, Proficy Webspace, and then click Stop Proficy Webspace Server.
  2. Wait a few moments for the action to complete. A command window opens briefly and then closes.
  3. On the Start menu, point to Programs, Proficy Webspace, and then click Start Proficy Webspace Server.
  4. Wait a few moments for the action to complete. A command window opens briefly and then closes.