Access BOM Items

About this task

An operation contains a list of BOM items necessary to perform the operation. As an operator, you can access the BOM section to specify the consumption of the BOM items for a product.

Procedure

  1. Select the operation whose BOM items you want to access.
  2. Select BOM.
    The BOM section appears, displaying the BOM items associated with the selected operation.

    The number of the BOM tab indicates the total number of mandatory BOM items that are yet to be consumed to complete the operation on the serial/lot.

    In Unit Operations, the number of the BOM tab indicates the total number of mandatory BOM items that are yet to be consumed to complete the operation on the serial/lot. In Work Queue, the number on the BOM tab indicates the total number of mandatory BOM items that are yet to be consumed to complete the operation on all the serials/lots that you have clocked on for the operation. The following table provides information on each column in the table.
    ColumnDescription
    ORDERThe recommended order of consumption of the BOM item in an operation.
    MATERIALThe material number of the BOM item.
    MATERIAL DESCThe material description of the BOM item.
    REQ QTYThe planned quantity of the BOM items required for the completion of the serial/lot for the operation.
    CONSUMED QTYThe actual quantity of the BOM items consumed during the production.
    UOMThe unit of measure (UOM) of the BOM item.
    SERIAL/LOT#The serial/lot of the raw material that was consumed.
    LOWER QTY The lower tolerance quantity of the BOM item that can be consumed.
    UPPER QTY The upper tolerance quantity of the BOM item that can be consumed.
    SCRAP FACTOR The Percentage of this BOM item that is expected to be lost during production of the formulation. For example, if 100 units of Product XYZ is required with a scrap factor of 1%, then you should have a 101 units on hand when preparing to produce the product.
    STORAGE UNIT Unit currently storing the selected product.
  3. In the BOM section, select an item.
    The page containing the item details and consumption history appears.