About Clocking on Serials/Lots for an Operation
When an operation is created in Route Editor or the ERP system, if it is specified that the operation requires clocking on, you must clock on the serial/lot on which you want to work. It indicates that the you are ready to accept the work and perform the operation.
Operations are planned for execution in one or more production units during production. You can, however, clock on serials/lots for an operation only in one production unit.
- The operation is no longer available in the other production units.
- A timer is enabled to monitor the time you spent on the completion of an operation. The time you spent on an operation is visible only to you. The completion time of an operation may differ from one operator to another.
- A clock-on status indicator appears for the operation.