Before you begin
Access the receiver for which you want to generate samples. You can generate samples only for a material lot for which inspection tests are defined in
Plant Applications Administrator (indicated by

).
Procedure
- In the left pane, under the receiver, select the material for which you want to generate samples.
The Edit Traceability section appears.
- If you do not want to split the lot:
- Enter a number in the ACTUAL SL/LOT# column.
- Enter the quantity in the QTY column.
- If you want to split the lot:
- In the ACTUAL SL/LOT# column, select
.A new row appears for the sublot. Repeat this step depending on the number of sublots you want to create.
- For each sublot, enter a value in the ACTUAL SL/LOT# column. This value must be unique for the lot.
- For each sublot, enter the quantity in the QTY column.
- As needed, enter values in the remaining fields.
-
Select Save.
Changes to the lot are saved.
Note: You can continue to change the lots
until the inspection begins. After you enter the inspection criteria, you
cannot change the lots.
-
Select Generate Samples.
The Generate Samples button is enabled only if the sum
of the quantities of all the sublots is equal to the total number of items in
the lot.
Samples are generated for the lot or each sublot and appear in the
Inspection Criteria section. The size of the sample is
calculated based on the size of the lot or sublot. The status of the receiver
changes to awaiting inspection (indicated by

).