STATUS | The status of the defect for which a non-conformance has been created. |
SERIAL/LOT# | The serial/lot number for which the non-conformance has been created. |
OP | The operation during which the non-conformance has been created. |
DISP | The disposition method implemented on the serial/lot. If the serial/lot is yet to be disposed, the value in this column is blank. |
MATERIAL | The material of the serial/lot. |
MATERIAL FAMILY | The material family associated with the material. |
MATERIAL DESC | The description of the material. |
CTP/REWORK OP | The operation until which the serial/lot can be processed if the disposition method is Continue to Process (CTP). |
ACTIONS | Contains the following buttons: : Select this button to access the non-conformance details. : Select this button to access the defect history.
|