historianTagMaxCacheSize | Enter the maximum cache size in KB. The default value is 50000 .Example: historianTagMaxCacheSize=50000 |
historianTagCacheTimeOut | Enter the duration in the format duration<timeformat> after which the cached Historian tags are cleared by the mes-dataservice-impl microservice. Where: <timeformat> is h , m , or s to indicate time in hours, minutes, or seconds, respectively. The default value is 6h .Example: historianTagCacheTimeOut=6h |
scheduler.tagcaching.seconds | Enter the duration in seconds after which the Historian tags are cached again by the mes-dataservice-impl microservice. The default value is 21600 .Example: scheduler.tagcaching.seconds=21600 |