Clear |
If this is the only disposition method specified for the lot:
- The status of the defect is set to Not a Defect, indicated
by
.
- The hold on the serial/lot is released.
If the disposition methods also include Use as is or Scrap (but
do not include MRB, Continue to Process, or Rework):
- The status of the defect is set to Closed, indicated by
.
- The hold on the serial/lot is released.
If the disposition methods also include MRB, CTP, or Rework:
- The status of the defect is Active, indicated by
. When the defect is in the Active
status, the hold on the serial/lot is released.
- In the case of CTP or Rework, when the operation specified
in the USE UNTIL/REWORK OPERATION box
is reached, the serial/lot will be placed on hold. The
defect status is changed to Planned, indicated by
.
|
Continue to process (CTP) |
- The status of the defect is Active, indicated by
. When the defect is in the Active
status, the hold on the serial/lot is released.
- When the operation specified in the USE
UNTIL/REWORK OPERATION box is reached, the
serial/lot will be placed on hold. The defect status is
changed to Planned, indicated by
.
|
Use as is |
If the disposition methods for the lot do not include MRB,
Rework, or CTP:
- The status of the defect is set to Closed, indicated by
.
- The hold on the serial/lot is released.
If the disposition methods for the lot include MRB, Rework, or CTP:
- The status of the defect is Active, indicated by
. When the defect is in the Active
status, the hold on the serial/lot is released.
- In the case of Rework or CTP, when the operation specified
in the USE UNTIL/REWORK OPERATION box
is reached, the serial/lot is placed on hold. The defect
status is changed to Planned, indicated by
.
|
Scrap |
If the disposition methods for the lot do not include MRB,
Rework, or CTP:
- The status of the defect is set to Closed, indicated by
.
- The hold on the serial/lot is released.
If the disposition methods for the lot include MRB, Rework, or CTP:
- The status of the defect is Active, indicated by
. When the defect is in the Active
status, the current serial/lot will be released from
hold.
- In the case of Rework or CTP, when the operation specified
in the USE UNTIL/REWORK OPERATION box
is reached, the serial/lot will be placed on hold. The
defect status is changed to Planned, indicated by
.
|
Rework |
- The status of the defect is set to Active, indicated by
. After completion of the
rework operation, the status is changed to Planned,
indicated by .
- The serial/lot continues to be on hold. The hold is released
after the completion of rework.
|
MRB |
- The status of the defect is set to Active, indicated by
.
- The serial/lot continues to be on hold.
|