Supported Schema Versions
- Work orders
- Process orders
- Materials
- Material lots
- Outside Processing (OSP)
Work Orders
- Schema Version 6: You can provide the following values:
- Upper and lower tolerances of a BOM item and their precision
- Scrap factor (the percentage of the product that is predicted to be scrapped)
- Precision of the quantity of the product
- The default storage unit of a BOM item
allowManualSkip
in thebehaviours
array for the operation. If you do so, the operator can choose to skip the operation while executing the work order. If, however, you set theskipifSuccessorStarted
parameter to true, the operation will be automatically skipped when the next operation is ready. - Schema version 5: You can override the following route components in
a work order:
- BOM items of a route
- BOM items of individual operations in a route
- Values of BOM item properties
- Values of route-level and operation-level properties
- Schema version 4: You can import work orders for serialized as well as non-serialized products with or without route definition.
- Schema version 3: You can import work orders for serialized products with or without route definition.
Materials
- Schema version 3: You can import materials for serialized as well as non-serialized products.
- Schema version 2: You can import materials for serialized products.
Material Lots and Outside Processing (OSP)
- Schema version 4: You can update the status, quantity, and properties of a material lot.
- Schema version 3: You can import material lots and OSP details - providing the status is not mandatory.
- Schema version 2: You can import material lots and OSP details - providing the status is mandatory.
Process Orders
- Schema version 2: You can provide values of the process order
properties. If the process order is not yet started, it is deleted and a new
one is created with the properties and values that you provide in the
process order import document (POID).
In addition, providing the production line is not mandatory, and you can include production lines with multiple execution paths. When a production line has multiple execution paths, the process order becomes an unbound process order. You can associate a production line with an execution path using Plant Applications Administrator or Plant Applications Web Client; or you can leave it as is.
- Schema version 1: You can import process orders containing information about the planned quantity, material, production line, and planned start and end dates.