Configuration Parameters in the ERP Export Service
As a system administrator, you can configure the following parameters in the ERP Export service and the Property Definition application in Plant Applications Web Client.
docker-compose -f erpexportservice.yml config > PAErpExportService.yml
docker stack deploy -c PAErpExportService.yml PAErpExportService
If you have installed Standard Plant Applications Web Client, these parameters are available in the following file: C:\Program Files\GE Digital\PlantApplicationsWebClient\config-repo\erp-export-service\prod\<version>\erp-export-service-prod.properties. After you change the values of parameters, restart the ERP Export service.
Parameter | Description |
---|---|
erp.outbound.messages.messageType | The format of the message. Provide one of the following
values:
|