Configuration Parameters to Import a Material
As a system administrator, you can configure the following parameters in the ERP Import service to import a material.
docker-compose -f erpimportservice.yml config > PAErpimportservice.yml
docker stack deploy -c PAErpimportservice.yml PAErpimportservice
If you have installed Standard Plant Applications Web Client, these parameters are available in the following file: C:\Program Files\GE Digital\PlantApplicationsWebClient\config-repo\erp-import-service\prod\<version>\erp-import-service-prod.properties. After you change the values of parameters, restart the ERP Import service.
Parameter | Description |
---|---|
Material.property.group.id | The GUID of property group with the name Material Import from Property Definition application. This group Id belongs to Material Import. The default value is 79433EC1-6683-4BED-B353-BD667210E0A2. |