Configuration Parameters to Import a Process Order
As a system administrator, you can configure the following parameters in the ERP Import service to import a process order. If you want to change the values of these parameters, you must do so while installing Plant Applications Web Client, and then restart the ERP Import service.
docker-compose -f erpimportservice.yml config > PAErpimportservice.yml
docker stack deploy -c PAErpimportservice.yml PAErpimportservice
If you have installed Standard Plant Applications Web Client, these parameters are available in the following file: C:\Program Files\GE Digital\PlantApplicationsWebClient\config-repo\erp-import-service\prod\<version>\erp-import-service-prod.properties. After you change the values of parameters, restart the ERP Import service.
Parameter | Description |
---|---|
processorder.property.group.id | The GUID of property group with the name ProcessOrder Import from the
Property Definition application. This group Id belongs to ProcessOrder
Import. The default value is 8a290266-bd40-4508-a0d8-3793d72e010b. |