Create an Operation

About this task

An operation is an activity that consists of steps that you perform while producing a product.

You can create operations in a route that is in the draft state. However, if you want to create an operation in a released or archived route, you must first revise the route.

When you create an operation, you can set the sequence of the operation, and select the equipment used for that operation.

This topic describes how to create an operation. You can also copy an existing one.

Before you begin

Create a route.

Procedure

  1. In the Route Editor page, select the route for which you want to create an operation.
    The Edit Route page appears, displaying a list of operations in the route.
  2. Select .
    A blank row appears in the Overview section.
  3. Provide values as specified in the following table.
    ColumnDescription
    SEQ

    Enter the sequence number of the operation. By default, the value in this column for the first operation is 1. The default sequence numbers of the subsequent records are automatically incremented by 10. However, you can modify this sequence number as per your requirement. This gap allows you to add new operations between two operations without the need to modify the sequence numbers of all the operations. If you want to perform multiple operations simultaneously (that is, for parallel tasks), provide the same sequence number.

    NAMEEnter a unique name for the operation that does not exceed 100 characters.
    Note: The name must be unique among all operations in the route.
    DESCRIPTIONEnter a description for the operation that does not exceed 1000 characters.
    BEHAVIORSelect the behavior of the operation. The following options are available:
    • Non Clocking: Select this option if the operation does not require a manual clocking on. If you select this option, you can mark an operation complete even if serials/lots are not clocked on, mandatory BOM items are not consumed, or values for mandatory quality variables are not specified.
    • Clocking: Select this option if the operation requires manual clocking on and clocking off. By default, Clocking is selected for an operation.
    LABOR TYPESSelect the labor types for the operation. A value is required.
    Note: If the behavior of the operation is set to Non Clocking, this field is disabled.
    DEFAULT LABOR

    Select the default labor type. A value is required. You can choose from the list of values that you selected in the LABOR TYPES column.

    When an operator clocks on a serial/lot number using the Work Queue or Unit Operations application, by default, the labor type that you select in this column is selected. The operator can, however, choose a different one from the ones that you selected in the LABOR TYPES column.
    Note: If the behavior of the operation is set to Non Clocking, this field is disabled.
    EQUIPMENT

    Select the equipment that is used to perform the operation. You can select multiple pieces of equipment for the same operation, and you can select the same piece of equipment for multiple operations.

    When you select multiple pieces of equipment, the selected number appears. You can select the drop-down list box to view the selected pieces of equipment.

    Tip: You can also select the equipment used in an operation from the Resources section.

Results

The operation is created and added to the route.

What to do next

Link a BOM item to the operation.