Creating a Production-Based Waste Event
You can track the waste that was generated for a specific production event. A production-based waste event is tagged to the event number.
Procedure
- Access the Waste page.
- The EVENT TIME is the date and time of creating the waste event record.
- Select
and select Add Production Based Waste Event.
- In the VIEW BY box, select the time range to retrieve the events.
- Select the EVENT box to select an event for which you want to create a waste record.By default, 500 records will be displayed. As you scroll down and reach the end of the list, you can select More to display 500 more records.
- In the LOCATION box, select the source of the specific equipment that generated the waste.
- In the AMOUNT field, enter the amount of waste that was generated.
- In the MEASURING UNITS box, select the unit of measurement to correspond with the amount of generated waste.
- In the WASTE TYPE box, select the category of waste as configured in the waste model that you created in Plant Applications Administrator.
- In the FAULT box, select the error that led to the generation of waste.
- In the REASON box, the reason is auto populated based on the error selected in the FAULT box.Note: The reasons are configured in Plant Applications Administrator.
- In the ACTION box, select the corrective action that was taken to fix the fault.
- Optional: In the ADD COMMENT field, enter a comment or observation and select Save.