hist<n>.service.origin | Enter the IP address of the GE Proficy Historian Server. For example, 10.181.213.204 . |
hist<n>.service.port | Enter the port number on which the GE Proficy Historian Server is installed. Tip: You can leave this property blank if the GE Proficy Historian Server is installed on the default port 8443. |
hist<n>.service.hostname | Enter the host name of the GE Proficy Historian Server as configured in the Plant Applications Administrator. For example, GESERVER . |
hist<n>.service.client_id | Enter the client id of the Historian Administrator. - Historian 7.0: admin is the default.
- Historian 8.0 or later: <hostname.admin> where the host name is the name of the server where the Historian web tools are installed.
|
hist<n>.service.client_secret | Enter the client secret of the Historian Administrator. |
hist<n>.uaa.origin | Enter the host (NetBIOS) name of the Historian UAA server. Note: The fully-qualified domain name (FQDN) is not supported. |
hist<n>.uaa.port | Enter the port number on which the Historian UAA server is installed. |