Add a UAA User

About this task

You must add User Authentication Service (UAA) users to access the Plant Applications Web Client.

Procedure

  1. Log in to the computer where you installed the Plant Applications Web Client.
  2. Select Start, and then search for the Command Prompt application.
  3. In the search results, right-click Command Prompt, and then select Run as administrator.
  4. In the command prompt, modify the directory path to the path where the PA_UAA_Config_Win.bat file is located.
    Note: By default, the PA_UAA_Config_Win.bat file is located in the Plant Applications Web Client installation directory.
  5. In the command prompt, enter PA_UAA_Config_Win.bat.
  6. Press Enter to run the PA_UAA_Config_Win.bat file.

Results

The user is added as a UAA user to the Operations Hub UAA with an access level you set for the user in the PA_UAA_Config_Win.bat file.