Add a User-Defined Event
Procedure
- Log in to Plant Applications Web Client.
-
In the application navigation menu, select
.
The Open page appears. -
Select
, and then select User Defined Event.
The Add User Defined Event window appears, displaying a list of user-defined autolog sheets accessible to you as configured in Plant Applications Administrator. - In the Choose activity section, select an activity to create a user-defined event on the selected activity.
- In the Add Event Details section, in the EVENT NUMBER box, enter a unique event number.
- In the DURATION box, select a start and end time for the event.
- Optional:
Specify values for the following properties: STATUS, APPLIED PRODUCT, and COMMENT.
Note: When the status of a user-defined event associated with the activity is set to a production status that has the Lock Event Data option enabled, you do not have the privilege to modify the autolog sheet for that event.
- In the REASONS box, select a reason to create a user-defined event.
- Select Save.