Default Categories, Groups and Properties

The following table includes the default categories, groups and properties defined in the ERP and Route Editor applications:

CategoryGroupProperty
ERP AppMaterial Import
  • unitofmeasure
ERP AppMaterialLot Import
  • Receive Line
  • Receiver Status
  • Receiver Unit
  • Inventory Line
Route AppWorkOrder ImportNo default properties
Note: Do not delete the aforementioned Categories, Groups and Properties that appear in the Property Definition by default.

The above properties can be used in the respective applications to store, process, and analyze data.

Example: The value of the unitofmeasure property is set by the ERP import for materials.

You can also create more property definitions in the aforementioned groups as required.

Example: When you import a material, if you require more information on the material , you can add more property definitions in the Material Import group to capture and utilize that information. Refer to Create a Property Definition.