About Status Indicators
A status indicator is a color-coded icon that provides the status of a work order, operation, or a serial/lot. The progress of work of all the serials/lots and operations indicates the overall status of a work order. The following table provides information on the status indicators for a serial/lot, operation, and a work order.
Note: During production, the status of an operation may differ as follows:
- When a serial/lot is on hold, the status of the operation associated with that serial/lot can be In Progress.
- When a serial/lot is scrapped, the operation in which the serial/lot is scrapped along with all subsequent operations that were configured to be performed on the serial/lot is Cancelled.
Status | Status Indicator | Description for a Serial/Lot | Description for an Operation | Description for a Work Order |
---|---|---|---|---|
Not Ready | ![]() | Not applicable | Indicates that none of the serials/lots are available for you to begin the operation. | Not applicable |
Ready | ![]() | Indicates that no operation has been performed on the serial/lot yet, and the serial/lot is ready for you to perform the operation. | Indicates that you can begin work for the operation. | Indicates that you can begin work for the work order. |
In Progress | ![]() | Indicates that work has begun on the serial/lot (that is, the serial/lot is clocked on or was clocked on in the past). | Indicates that work for the operation has begun on at least one serial/lot (that is, at least one serial/lot is clocked on for the operation or was clocked on the past). | Indicates that work has begun for at least one serial/lot in the work order (that is, at least one serial/lot in the work order is clocked on or was clocked on in the past). |
On Hold | ![]() | Indicates that a defect has been created for the serial/lot. After the defect is closed, the status is changed to the previous status. | Indicates that the operation is on hold. For example, if the disposition method specified for a defect is Continue to Process (CTP), and the defect is re-evaluated during a future operation, that future operation is on hold. When the serial/lot is ready for that future operation, the operation status is Ready or In Progress, and the serial/lot status is On Hold. | Not applicable |
Cancelled | ![]() | Not applicable | Indicates that the operation is in the Cancelled status. For example, when a serial/lot is scrapped or split, the status of the current operation on the serial/lot is changed to Cancelled. | Indicates that the work order is cancelled. |
Scrapped | ![]() | Indicates that the serial/lot has been scrapped. | Not applicable | Not applicable |
Split |
![]() | Indicates that the lot has been split up. This happens when a non-conformance has been created on some of the items in the lot. | Not applicable | Not applicable |
Completed | ![]() | Indicates that all operations for the serial/lot are completed. | Indicates that the operation is completed for all serials/lots. | Indicates that all the operations associated with all the serials/lots in the work order are completed. |