About Status Indicators
A status indicator is a color-coded icon that provides the status of a defect. The status of a defect depends on the status and method of disposition specified for the serial/lot. The following table provides information on the status indicators of a defect created on a serialized or a non-serialized product.
Status | Status Indicator | Description for a Serialized Product | Description for a Non-Serialized Product |
---|---|---|---|
Submitted | Indicates that the defect is submitted for disposition. This status indicator appears when the defect is not yet disposed. | Indicates that the defect is submitted for disposition. This status indicator appears when the defect is not yet disposed. | |
Active | Indicates that the disposition method is MRB, Rework, or Continue to process (CTP). | Indicates that one of the disposition methods for the lot is MRB, Rework, or CTP. | |
Planned | Indicates that the disposition method is Rework or CTP and the serial/lot has reached the operation specified in the USE UNTIL/REWORK OPERATION box. | Indicates that one of the disposition methods for the lot is Rework or CTP and the serial/lot has reached the operation specified in the USE UNTIL/REWORK OPERATION box. | |
Not a defect | Indicates that the defect is considered invalid. This status indicator appears when the disposition method is Clear. | Indicates that the defect is considered invalid. This status indicator appears when the only disposition method for the lot is Clear (that is, no other disposition methods have been specified for the lot). | |
Closed | Indicates that the disposition method for the defect is Use as is or Scrap. | Indicates that the disposition methods for the lot include Use as is and Scrap, but do not include MRB, Rework, or CTP. |