SQL Server Requirements
SQL Server Installed Components
- Database Engine Services
- Reporting Services
- Client Tools Connectivity
- Client Tools Backwards Connectivity
- SQL Server Books Online (recommended)
- Management Tools - Basic
SQL Server Naming Conventions
Do not use special characters for server names.
Supported Network Protocols
Before installing SQL Server, the stand-alone named and default instances must support the following network protocols:
- Shared memory (Shared memory is not supported on failover clusters)
- Named pipes
- TCP/IP
- VIA
The same network protocol must be set up on the server and client computers to be able to communicate with each other.
SQL Server Browser Service and Plant Applications Server
If you are installing Plant Applications Server on a server with Microsoft SQL Server, the SQL Server Browser service (sqlbrowser) must be running before installing Plant Applications Server.
For information on SQL Server Browser service, go to the MSDN web site: http://msdn2.microsoft.com/en-us/library/ms165724.aspx
Enabling TCP/IP and XP_cmdshell
The xp_cmdshell option and the TCP/IP protocol, which are disabled by default, must be enabled. The installation process will verify whether the TCP/IP protocol is enabled and if it is not enabled, a message box appears asking permission to enable the TCP/IP protocol. If permission is denied, the installation process will quit. The xp_cmdshell option is automatically enabled during the installation process.