After installing the Plant Applications Server, the Plant Applications Server services should start automatically.
About this task
Verify that the Plant Applications Server services have started.Procedure
- Open the Windows Control Panel, and double-click Administrative Tools.
- Double-click Services.
- Scroll through the list of services and verify that the Plant Applications Server services have all started. If they have not started, start them manually.
Another method for verifying that the
Plant Applications Server services have started is to view the server log files. These text files are created during the
Plant Applications Server installation. Each service has its own log file. By default, the log files are located on the
Plant Applications Server in the following directory:
C:\<Program Files>\Proficy\Proficy Server\LogFiles