Server Hardware Requirements
The minimum server requirements when running a Plant Applications environment without SOA entities and not using the Client or Workflow:
- 4 CPUs with 3.0 GHz processor each
- 16 GB RAM (Optimization of memory allocation needs to be to SQL Server)
- 1 TB hard drive (minimum 7.2KRPM)
For a standard implementation, GE recommends the following:
- 10 Cores with 2.6GHz processor each
- 32 GB RAM (Optimization of memory allocation needs to be to SQL Server)
- 4 TB hard drive (minimum 7.2KRPM)
Note: Hard drive size is dependent upon anticipated database growth, backups, and practices employed to purge data.