Set Up Languages for Plant Applications Displays
After installing Plant Applications, you can implement support for additional languages using its Native Language Support (NLS) features.
Procedure
- Select All Programs from the Windows Start menu.
- In the Proficy folder, select Configure Plant Applications Language Support. Alternatively, you can also run ConfigurePALanguages.exe located at <installation_directory>\Proficy\Proficy Workflow\Program to set up language support.
- At the Configure Plant Applications Database screen, modify any server settings as needed.
- Select one or more languages to include, then click Save. Tip: Use these options to set up language support after any subsequent Service pack or SIM upgrade.