Customize Your Application
You can edit the values in the Plant Applications configuration file to customize your installation.
Procedure
Change any of the following parameters in the configuration file as needed.
Parameter | Description |
---|---|
EventNumIsNumber | For the Excel Add-in to translate numeric values, set this value to True . The default value is False . See the EventNumIsNumber site parameter in the Plant Applications Help. |
ProdCodeIsNumber | For the Excel Add-in to translate numeric values, change this value to True. (The default value is False.) See the ProdCodeIsNumber site parameter in Plant Applications Help. |
AllowPasswordSave | To prevent users from saving their client passwords to local workstations, change this value to False. The default value is True. See AllowPasswordSave in the Plant Applications Help. |
LanguageNumber | By default, the site language is set to U.S. English. To change the default language, edit this value. See the LanguageNumber parameter in the Plant Applications Help. |
StartupSetBack | By default, the Event Manager service looks back three days (4320 minutes) to look for events at startup. To change this interval, edit the EventMgr system value. The suggested configuration is 6 to 12 hours. Services must be restarted for changes to take effect. See the System Users in Plant Applications Help. |
SpecificationSetting | The Autolog display uses this parameter to color-code test values by comparing them to the specification limits defined for each variables. When the value is 1 (the default) and the Test Values limit is greater than the Triggering Specification Limit, it triggers a specification flag updating the Test Values Color. When the value is 0 and the Test Values limit is greater than or equal to the Triggering Specification Limit, it triggers a specification flag updating the Test Values Color. |
UseProficyClient | Set this site parameter to True to merge the Plant Applications and SOA equipment models using the Workflow Client. Refer to Enabling the Proficy
Client UI and Aspecting in the Plant Applications Help. |
MinEventTimeSpan | To reduce the frequency of event generation, set this value to 0 . The default value of this parameter is four minutes. For more information, see the MinEventTimeSpan site parameter in the Plant Applications Help. |