ERP Integration Database Schema
The ERP Integration database stores messages that specify work orders, process orders, and materials. Messages are stored in the erp_integration_inbound_messages table until they are imported into the Plant Applications database. The following table describes the columns in the erp_integration_inbound_messages table.
Column | Description |
---|---|
Id | A system-generated identity value. |
Message_Type |
The identifier for the type of the record. This column contains one of the following values:
|
Media_Type |
The MIME type of the message. This column contains one of the following values:
|
Key_Data | The information added by the ERP Scheduler service when the record is processed (for example, work order number). The data can be used by system administrators for internal purposes, such as to query how many times the order number has been sent for import. |
Inserted_Date | The date and time (in UTC format) when the ERP system added the record to the table. |
Process_Start_Date | The date and time (in UTC format) when the ERP Scheduler service started processing the message. |
Process_Complete_Date | The date and time (in UTC format) when the ERP Scheduler service completed processing the message. |
Response_Code | The HTTP response code from the import process. |
Response_Message | The message that contains information about whether the import has been successful. |
Message |
The record that contains the details of the work order, process order, or material in a JSON, B2MML, or XML format. If the message is in the JSON format, this column contains one of the following files:
|
Inserted_By | The user who created the record. |