Troubleshooting Issues While Importing
First-Time Import of Material Lots from an ERP Application Fails
Possible root cause: The statuses of the material lots are not defined in Plant Applications Administrator.
- Access Plant Applications Administrator.
- Under Global Configuration, right-click Administer Production Status, and then select Edit.
- Select New Status, and provide values for the UNASSIGNED production status as shown in the following image:
- Select New Status again, and provide values for the OPEN production status as shown in the following image:
Possible root cause: The inventory line is not defined in Property Definition.
Resolution: If you have installed Plant Applications for the first time, set a value for the inventory.line property group using Property Definition in Plant Applications Web Client.
Possible root cause: Mismatch in units of measure
Resolution: The units of measure provided for each material lot in the message must match the units of measure for one of the units in the inventory line in Plant Applications. If it does not match or if multiple units have the same units of measure, an error occurs. In addition, this unit must contain the same OrgCode that you will provide in the material lot import document (MLID).