Cost Benefit Analysis Report for Sites
About the Cost Benefit Analysis Report for a Site
The Cost Benefit Analysis Report for a site enables you to analyze the cost avoided by resolving the cases that were created for the assets in the site. This includes the cases that were resolved for the blocks within the site. You can specify the period for which you want to view the report in the header section of the page. The report provides the following information for the specified period:
- The total number of cases created for the site and the total cost saved by resolving these cases.
- The avoided cost based on the site breakup, cases, and the categories and closure codes of the cases.
- Breakdown of the avoided cost for each case.
- List of all the cases that were resolved for the site, along with links to access the details of the cases.
- List of the five highest cost saving cases of the site.
The information in the report is presented using graphical elements such as charts and tables. This makes it convenient to analyze the information. The report is divided into the following sections to segregate the information for better analysis:
All monetary values in the report are displayed in the currency configured for the site and it appears in the Currency field in both the sections of the report.
For information on accessing the Cost Benefit Analysis Report for a site, refer to the Access the Cost Benefit Analysis Report topic.
The following image shows an example of the Cost Benefit Analysis Report for a site:

About the Total Cases & Avoided Cost Section
The Total cases & Avoided cost section in the Cost Benefit Analysis Report for a site contains the following items:
- Total cost avoided for the site
- This information appears in the Total Avoided cost for <Site Name> (<Currency>) field at the top of the Total cases & Avoided cost section.
- Bar chart displaying avoided cost
- The bar chart appears in the View the Avoided cost based on section. This chart provides a graphical comparison between the number of cases and avoided cost for each case closure code and site breakup. By default, the bar chart displays the data based on the closure codes of cases. However, you can select Site Breakup to view the data based on the site breakup.
- Pie chart displaying Cost Benefit Analyses of cases
- The pie chart appears in the View the CBA based on section. This chart provides a visual comparison between the proportions of cost avoided for each closure code and category of cases. By default, the pie chart displays the Cost Benefit Analysis data based on the closure codes of cases. However, you can select Case Category to view the data based on the case categories.
- Table containing details and cost breakdown of all cases resolved for the site
- This table contains the case IDs, description, and closure code of all the cases that were resolved for the site. Additionally, the table contains the breakdowns of the cost that was saved by resolving the cases, along with links to view the details of each case. The table contains the following columns:
- CASE ID
- CASE DESCRIPTION
- CLOSURE CODE
- PRODUCTION AVOIDED COST
- MECHANICAL AVOIDED COST
- TOTAL AVOIDED COST
About the Top 5 Cases Section
The Top 5 Cases section in the Cost Benefit Analysis Report for a site contains the following:
- Total cost avoided for the site
- This information appears in the Total Avoided cost for <Site Name> (<Currency>) field at the top of the Top 5 Cases section.
- Table containing details and cost breakdown of the five highest cost saving cases
- This table contains the case IDs, description, and closure code of all the five highest cost saving cases that were resolved for the site. Additionally, the table contains the breakdowns of the cost that was saved by resolving the cases, along with links to view the details of each case. The table contains the following columns:
- CASE ID
- CASE DESCRIPTION
- CLOSURE CODE
- PRODUCTION AVOIDED COST
- MECHANICAL AVOIDED COST
- TOTAL AVOIDED COST