Cost Benefit Analysis Report for Blocks
About the Cost Benefit Analysis Report for a Block
The Cost Benefit Analysis Report for a block enables you to analyze the cost avoided by resolving the cases that were created for the assets in the block. You can specify the period for which you want to view the report in the header section of the page. The report provides the following information for the specified period:
- The total number of cases created for the block and the total cost saved by resolving these cases.
- The avoided cost based on the block breakup, cases, and the categories and closure codes of the cases.
- Breakdown of the avoided cost for each case.
- List of all the cases that were resolved for the block, along with links to access the details of the cases.
- List of the five highest cost saving cases of the block.
The information in the report is presented using graphical elements such as charts and tables. This makes it convenient to analyze the information. The report is divided into the following sections to segregate the information for better analysis:
All monetary values in the report are displayed in the currency configured at the site level of the asset hierarchy and it appears in the Currency field in both the sections of the report.
For information on accessing the Cost Benefit Analysis Report for a block, refer to the Access the Cost Benefit Analysis Report topic.
The following image shows an example of the Cost Benefit Analysis Report for a block:

About the Total Cases & Avoided Cost Section
The Total cases & Avoided cost section in the Cost Benefit Analysis Report for a block contains the following items:
- Total cost avoided for the block
- This information appears in the Total Avoided cost for <Block Name> (<Currency>) field at the top of the Total cases & Avoided cost section.
- Bar chart displaying avoided cost
- The bar chart appears in the View the Avoided cost based on section. This chart provides a graphical comparison between the number of cases and avoided cost for each case closure code and block breakup. By default, the bar chart displays the data based on the closure codes of cases. However, you can select Block Breakup to view the data based on the block breakup.
- Pie chart displaying Cost Benefit Analyses of cases
- The pie chart appears in the View the CBA based on section. This chart provides a visual comparison between the proportions of cost avoided for each closure code and category of cases. By default, the pie chart displays the Cost Benefit Analysis data based on the closure codes of cases. However, you can select Case Category to view the data based on the case categories.
- Table containing details and cost breakdown of all cases resolved for the block
- This table contains the case IDs, description, and closure code of all the cases that were resolved for the block. Additionally, the table contains the breakdowns of the cost that was saved by resolving the cases, along with links to view the details of each case. The table contains the following columns:
- CASE ID
- CASE DESCRIPTION
- CLOSURE CODE
- PRODUCTION AVOIDED COST
- MECHANICAL AVOIDED COST
- TOTAL AVOIDED COST
About the Top 5 Cases Section
The Top 5 Cases section in the Cost Benefit Analysis Report for a block contains the following:
- Total cost avoided for the block
- This information appears in the Total Avoided cost for <Block Name> (<Currency>) field at the top of the Top 5 Cases section.
- Table containing details and cost breakdown of the five highest cost saving cases
- This table contains the case IDs, description, and closure code of all the five highest cost saving cases that were resolved for the block. Additionally, the table contains the breakdowns of the cost that was saved by resolving the cases, along with links to view the details of each case. The table contains the following columns:
- CASE ID
- CASE DESCRIPTION
- CLOSURE CODE
- PRODUCTION AVOIDED COST
- MECHANICAL AVOIDED COST
- TOTAL AVOIDED COST