Configure Plug-in Upgrades

A pre-requisite for successful custom plug-in upgrade in Operations Hub.

About this task

Plug-in developers can choose to write a specification, or use any transformation mechanism to get an EXE, JAR, or BAT file.

Procedure

  1. Prepare a data transformation for plug-in upgrade using any of these methods:
    Transformation File TypeDescription
    Jolt Open-source JSON-to-JSON transformation library written in Java.

    For more information, refer to https://github.com/bazaarvoice/jolt#Documentation

    For Jolt spec, you can use http://jolt-demo.appspot.com/ as a playground to test your transformation.

    JAR Java output using JSON transformation library such as https://mvnrepository.com/artifact/net.minidev/json-smart/2.4.7.
    For JAR, the plug-in upgrade infrastructure looks for the class to load. For example, public class GEBreadcrumb_3_0_0to3_0_1 wherein,
    • GEBreadcrumb is the plug-in name
    • 3_0_0 is the breadcrumb plug-in old version. The dot is replaced with an underscore.
    • 3_0_1 is the breadcrumb plug-in new version. The dot is replaced with an underscore.

    A transform instance is created for the class by invoking its static transform method: public static String transform(String inputJSON)

    .EXE Windows?? executable file. Create a transformation project with your choice of library (C++, Node, Python, etc.), which prints the transformed output json to console.
    For this executable,
    • 'FromVersion' schema input json is passed as command line argument
    • 'ToVersion' response JSON is read from its console output produced by the executable
    Note: Naming convention for the transformation file is <PluginName>-<FromVersion>-<ToVersion>-spec.json. For example GETrendCard-3.0.1-3.0.2-spec.json|jar|exe|bat.
  2. Log in to the machine where Operations Hub is installed.
  3. Place the plug-in transformation files in this location folder ..\ProgramData\GE\Operations Hub\iqp-config\plugin-transform-spec

Results

When Operations Hub administrator imports applications with old plug-ins, they are successfully upgraded to their latest versions.
  • The transformation engine looks for an incremental path of intermediatory transformation that can migrate a plug-in from a specific version to a desired version. For instance, GETrendCard-3.0.1-3.0.2-spec.json GETrendCard-3.0.2-3.0.4-spec.json GETrendCard-3.0.4-3.0.5-spec.json are used consecutively to upgrade plug-ins.
  • If incremental upgrades were not performed between Operations Hub versions, then the plug-in version may not remain subsequent for upgrade. For example, consider:
    • Operations Hub 1.7 has 3.0.1 version of GETrendCard
    • Operation Hub 2.5 has 3.0.5 version of GETrendcard

    The GETrendCard-3.0.1-3.0.5-spec.json file may not be available for upgrading plug-ins. In such cases, plug-in upgrades are not performed in Operations Hub.