Delete applications from Operations Hub.
About this task
- When you delete an application, only the application is deleted from Operations Hub. The
components used by the application are not
deleted.
- You cannot delete an application if it is locked.
- You cannot delete Operations Hub default
applications.
Procedure
- From the main navigation menu, select
APPS.
The
APPS workspace appears.
- In each row containing an application that you want to delete, select the check box.
- In the workspace heading, select , and then select Delete apps.
A message appears, asking you to confirm that you want to delete the applications.
Tip: Alternatively, in the row containing each application that you want to delete, select
, and then select
Delete app.
- Select OK.
The applications are deleted.