Check Box
The widget is available under designing application pages, drag-and-drop checkbox to a container. To use the old version, refer to Check Box.
. WhenProperty | Description |
---|---|
Target > Output Value | Selecting the check box in the end app sends value to the target. Use a query or a global to specify the target data source. |
Source > Input Value | Provides input for the check box from a data source. |
Source > Label (unchecked) | This is the label that appears when the check box is not selected. |
Source > Label (checked) | This is the label that appears when the check box is selected. |
Label Styling | Formats the label: Font Family, Font Size, and Font Color formats the label text. |
Check State Colors | Select colors that appear in the background of the check box.
|