Page Components
This topic describes the various UI components that you can use to design your page and configure the data.
Page Design
Field | Description |
---|---|
INPUTS | Contains UI components that receive input from application users. |
DISPLAY | Contains UI components that display information in the application. |
LAYOUTS | Contains UI components that are used to design a page layout. |
TOOLS | Contains UI components that allow application users to upload an Excel worksheet to load data into an entity, upload a list of devices in a CSV format, or manage events. |
INTEGRATION | Contains system plug-ins/widgets. |
CUSTOM | Contains custom UI plug-in components that have been uploaded by an application developer. |
Component Properties
Field | Description |
---|---|
Label | The text that appears for components such as check boxes and drop-down list boxes. |
Global Data | Allows the data to be available globally for use by other components or query inputs. This check box is enabled only after you specify an Id for the component. |
Allow Export | Indicates whether data that appears in the component can be exported. By default, this check box is cleared. |
Tooltips | Indicates whether data in a table cell should contain tooltips displaying the content. By default, this check box is cleared. |
Type | The data type of an input component. If you are configuring the settings of an component of the type graph or gauge, this field contains a list of graph or gauge types. |
Style | The style of a meter-type gauge component. |
Conditions | Applies a condition that executes an action at runtime. For
example, you can create a condition for the component/widget to
display a control button or a warning image if the temperature
recorded by the sensor exceeds 40 degrees Celsius. Select Add conditions to build and apply conditions. |
Hidden | Select the check box to hide the component/widget at runtime.
By default, this check box is cleared. When a component/widget is marked as hidden, it can be shown only on associating with a button using the toggle show/hide action. As a best practice, either use Conditions or Hidden. Avoid using these properties together. |
Show on | Indicates that the component/widget is visible in the selected devices. By default, the options Mobile, Tablet, and Desktop are selected. |
X-axis Label | The label of the horizontal axis of an component of the type graph. |
Y-axis Label | The label of the vertical axis of an component of the type graph. |
Required | Indicates whether it is mandatory to enter a value for the component that is used as an input to a query. By default, this check box is cleared. |
Target Data | The query input that is the target for the value of the component. |
Source | The source from which data should be retrieved to initialize
the component. If you are configuring the settings of an input
component, you can select one of the following options:
|
Group By | Enables to group the data in a graph by the selected tag name. |
Options | Indicates whether the values in the component are hard-coded or displayed dynamically from a query. |
Actions | The action that should be triggered when the component is selected. |
First Option | The first option that appears in an component of the type drop-down list box (for example, select an asset). |
Step | The step value used for a slider component. |
Minimum | The minimum value for an component that contains a range (such as a slider or a gauge). |
Maximum | The maximum value for an component that contains a range (such as a slider or a gauge). |
True Label | Customized text that appears when a toggle or an indicator is active. |
False Label | Customized text that appears when a toggle or an indicator is inactive. |
Width | The width of the component of the type toggle. |
Show <number> rows at a time | The number of rows that can appear at a time in an component of the type grid. |
Validation | The validations to be applied on the value entered in an
input component. You can select the following options:
|
Disabled | Indicates whether you want the component to appear as disabled in the application. |
Range Limit | The range of values that application users can enter in the component. |
Stacked | Indicates whether the bars displayed in an component of the type graph should be stacked. By default, this check box is cleared. |
Visual | |
Rounded Corners | Applies rounded corners for the selected component. |
Custom Colors | Select the check box to set these options:
|
Horizontal Alignment | Aligns the component left, right, or center. |
Columns/Rows | Allows to create a grid layout to design your pages. You can
split the page into vertical columns and horizontal rows for
better organization of page components. Enter the number of
columns/rows in the text box. You can add upto 36 columns and 6
rows. Tip:
|
Responsive | |
Responsive Pattern | Select how the container layout must respond on web pages. |