Slider
A slider is a graphical user interface element that is used to indicate an amount or value by means of an indication hash marker that can move on a horizontal plane that has a value indication. To use the new version, refer to Slider.
Slider Settings
- Source: The data source can be based on which queries have been added in the Page Data section. It is also possible to manually insert the data source or to use a formula.
- Required: Specify if an input must be sent to the query.
- Submit on Charge: If selected, changing the value of the input submits the query to which this input is assigned.
- Step: The spacing between variables on the horizontal plane of the slider.
- Minimum: Sets the minimum variable on the horizontal plane of the slider. This number appears on the left side of the plane.
- Maximum: Sets the maximum variable on the horizontal plane of the slider. This number appears on the right side of the plane.
Possible Uses
A slider can be used for any of the following purposes:
- To provide a number selector.
- To indicate the volume on an audio recorder or a maximum/minimum price.
- To allow a user to select a price they would be willing to pay as part of a filter system for search results.