Chart Line
The widget is available under designing application pages, drag-and-drop chartLine to a container.
. WhenProperty | Description |
---|---|
Line Type | Select from the available list of chart line types. |
Source > Data Source | Provide the input data source to receive values for the chart. |
Title | Title name for the chart. |
Subtitle | Subtitle name for the chart. |
Y Axis Title | Title name for y-axis. |
X Axis Title | Title name for x-axis. |
Legend | Select the Visible check box if you want to show the chart legend. You can also use the options to position the legend in the chart. |
Crosshair | Select the check box if you want to show the crosshairs in the chart. |
Show Points | Select the check box if you want to show data points in the chart. |
Point Symbol | Select from the available list of symbols to represent the points in the chart. |
Stacking |
|