While designing a page, you can use the Google Maps widget to display the locations of assets on a map. To do so, you require the API key generated by Google. This topic describes how to access the key and use it in the application that you want to create.
Procedure
- Access https://cloud.google.com/maps-platform/, and follow the on-screen instructions to generate the API key.
The API key is generated.
Note:
Ensure that the following APIs are enabled for the key:
- The Geocoding API
- The Maps JavaScript API
- At the Ubuntu server command prompt, enter
cd <path to the installation folder>
to change to the installation directory. - Enter
sudo nano endapp/config/config.js
to access the configuration file. - In the command line
gmapKey: '[GMAPSAPIKEY]'
, replace [GMAPSAPIKEY]
with the API key generated in step 1. - Save and close the file.
- Enter
sudo docker-compose restart endapp
to restart the endapp container.The Google Map widget is now available for use in the application. Asset locations are now displayed on a map.