About the Certificate Management Tool
The Certificate Management tool allows you to manage external certificates and renew expired certificates. It is installed automatically when you install Operations Hub.
Using the Certificate Management tool, you can manage the following types of certificates:
- Server certificates, which include local certificates and imported certificates.
- Issuer certificates, which include certificates that are trusted by Operations Hub. This is required to connect to an external UAA instance. If you want to connect to LDAP, use the LDAP service to generate the certificate. Typically, you will only require the root CA certificate.
Using the Certificate Management tool, you can perform the following tasks:
- Access a certificate.
- Renew a local certificate.
- Import a server certificate or an issuer certificate.
- Remove a server certificate or an issuer certificate.
- View log messages that are generated while managing the certificates.