Query Paths

About Query Paths

On the LOPA Overview page, when you select the tabs in the workspace, the following queries are executed:

  • LOPA Under Review Query: This query retrieves a list of LOPA that are not in the Complete state. This query is executed when you select the Under Review tab on the LOPA Overview page, and populates the Under Review section with the list of LOPA that is retrieved.
  • LOPA Approved Query: This query retrieves a list of LOPA that are in the Complete state. This query is executed when you select the Approved tab on the LOPA Overview page, and populates the Approved section with the list of LOPA that is retrieved.

You can, however, specify different search queries for LOPA by replacing the default queries.

Specify Different Query Path

About This Task

This topic describes how to specify different search queries for LOPA by replacing the default queries.

Procedure

  1. Access the LOPA Admin page.
  2. In the Query Paths workspace, next to the query that you want to replace, select the Select button.
    The Select a query from the catalog window appears.
  3. Navigate to the folder that contains the query that you want to specify.
  4. Select the query that you want to specify, and then select Open.
    In the box corresponding to the query that you want to replace, the complete path to the query that you selected appears.
  5. In the upper-right corner of the LOPA Admin page, select Save.
    The default query is replaced by the query that you selected.