Initiating Events

About Initiating Events

Initiating events represent the various types of causes that can result in a hazardous scenario. In LOPA, you can create an Initiating Event record for each type of initiating cause. When you create a LOPA, these records are used to populate the frequency of occurrence of the Initiating Event.

Default Initiating Event Records

By default, the following Initiating Event records are available in APM:

Initiating Event IDLower BoundaryUpper BoundaryDefault Value
Gasket/packing blowout1E-060.010.01
LOTO(lock-out-tag-out)0.00010.0010.001
Unloading/loading hose failure0.0110.01
Cooling water failure0.0110.01
Atmospheric tank failure1E-050.0010.001
Crane load drop0.00010.0010.0001
Piping residual failure-100m-Full Breach1E-061E-051E-05
Pump seal failure0.010.10.1
Piping leak(10% section)-100m0.00010.0010.001
Pressure Vessel Residual Failure1E-071E-051E-06
Large external fire(aggregate causes)0.0010.010.01
Safety valve opens spuriously0.00010.010.01
BPCS instrument loop failure0.0110.1
Regulator failure0.110.1
Operator failure0.00010.10.01
Small external fire(aggregate causes)0.010.10.1
Lightning strike0.00010.0010.001
Third party intervention(external impact by backhoe, vehicle, etc.)0.00010.010.01
Turbine/diesel engine overspeed with casing breach0.00010.0010.0001

Access an Initiating Event

Procedure

  1. Access the LOPA Admin page.
  2. In the left pane, select Initiating Events.
    A list of available Initiating Events appears.
  3. In the row for the Initiating Event that you want to access, in the Initiating Event ID column, select the link.
    In the Record Manager, the page for the selected record appears, displaying the datasheet for the record.
    Note: To modify the Initiating Event, as needed, modify values in the available fields, and then select to save your changes. The values in the existing LOPA and Hazards Analysis Cause records that have used the modified Initiating Event, will not be affected by the changes.
    • If you want to apply the changes to an existing LOPA, on the LOPA datasheet, in the Initiating Event Type box, you must reselect the Initiating Event that you modified.
    • If you want to apply the changes to an existing Cause, on the Hazards Analysis Cause datasheet, in the CCPS Cause Type box, you must reselect the Initiating Event that you modified.

Create an Initiating Event

Before You Begin

  • For the Initiating Event that you want to create, you must create a system code in the INIT_EVENT System Code Table. The System Code Table populates the Initiating Event ID box. When you create the Initiating Event, in the Initiating Event ID box, you must select the value that you entered in the System Code Table.

Procedure

  1. Access the LOPA Admin page.
  2. In the left pane, select Initiating Events.
    A list of available Initiating Events appears.
  3. In the upper-left corner of the workspace, select .
    A blank datasheet for Initiating Event appears.
  4. As needed, enter values in the available fields.
  5. In the upper-right corner of the workspace, select .
    The Initiating Event record is created.

Results

  • On the LOPA datasheet, the Initiating Event that you created appears in the list of values in the Initiating Event Type box.
  • On the Hazards Analysis Cause datasheet, the Initiating Event that you created appears in the list of values in the CCPS Cause Type box.

Delete an Initiating Event

Before You Begin

  • Before you can delete an Initiating Event, you must delete the corresponding System Code that you created in the INIT_EVENT System Code Table.

Procedure

  1. Access the LOPA Admin page.
  2. In the left pane, select Initiating Events.
    A list of available Initiating Events appears.
  3. In the row for each Initiating Event that you want to delete, select the check box.
    In the upper-right corner of the workspace, the button is enabled.
  4. Select .
    The Delete Initiating Events dialog box appears, asking you to confirm that you want to delete each selected Initiating Event.
  5. Select OK.
    Each selected Initiating Event is deleted.

Results

  • On the LOPA datasheet, the Initiating Event that you deleted does not appear in the list of values in the Initiating Event Type box.
  • On the Hazards Analysis Cause datasheet, the Initiating Event that you deleted does not appear in the list of values in the CCPS Cause Type box.
    Note: The values in the existing LOPA and Hazards Analysis Cause records that have used the deleted Initiating Event will not be affected when you delete the Initiating Event record.