Human IPLs
About Human IPLs
Human IPLs are IPLs that require operators or other staff to take action to prevent an undesired consequence, in response to alarms or following a routine check of the system.
In LOPA, you can create a Human IPL record for each type of human IPL. This record stores the recommended probability of failure on demand (PFD) of the human IPL. The PFD value indicates the likelihood that the Human IPL will fail to perform its safety function when required. The Human IPL records populate the IPL Sub Type field in the IPL Checklist section of the Safeguard, which is of type Human IPL.
Default Human IPL Records
By default, the following Human IPL records are available in APM:
Human IPL ID | Lower Range | Upper Range | Default Value |
---|---|---|---|
Human Action with BPCS/alarm-4 min response time | 0.01 | 1 | 0.1 |
Human Action with >10 min response time | 0.1 | 1 | 0.1 |
Human Action with >40 min response time | 0.01 | 0.1 | 0.1 |
Access a Human IPL
Procedure
Create a Human IPL
Before You Begin
-
For the Human IPL that you want to create, you must create a system code in the MI_HUMAN_IPL System Code Table. The system code populates the Human IPL ID box. When you create the Human IPL, in the Human IPL ID box, you must select the value that you entered in the System Code Table.
Procedure
Results
-
In the IPL Checklist section of the Safeguard of type Human IPL, the Human IPL that you created appears in the list of values in the IPL Sub Type box.
Delete a Human IPL
Before You Begin
-
Before you can delete a Human IPL, you must delete the corresponding System Code that you created in the MI_HUMAN_IPL System Code Table.
Procedure
Results
-
In the IPL Checklist section of the Safeguard of type Human IPL, the Human IPL that you deleted does not appear in the list of values in the IPL Sub Type box.
Note: The values in the existing Safeguards that have used the deleted Human IPL will not be affected when you delete the Human IPL record.