Consequence Probabilities
About Consequence Probabilities
Consequence Probabilities represent the probability of occurrence of various modifier types and are stored in the Consequence Adjustment Probability records. When you create a Conditional Modifier in LOPA, these records are used to populate the probability for the selected modifier type.
Default Consequence Adjustment Probabilities Records
By default, the following Consequence Adjustment Probabilities records are available in APM:
Modifier ID | Default Value |
---|---|
Probability of Ignition | 0.5 |
Probability of Escape and Incident | 0.5 |
Others | 0.5 |
Probability of person present | 0.5 |
Access a Consequence Probability
Procedure
Create a Consequence Probability
Before You Begin
-
For the Consequence Probability that you want to create, you must create a system code in the MI_CONSQ_ADJ_PROB System Code Table. The System Code Table populates the Modifier ID box. When you create the Consequence Probability, in the Modifier ID box, you must select the value that you entered in the System Code Table.
Procedure
Results
- On the Consequence Modifier datasheet, the Consequence Probability that you created appears in the list of values in the Type box.
Delete a Consequence Probability
Before You Begin
-
Before you can delete a Consequence Probability, you must delete the corresponding System Code that you created in the MI_CONSQ_ADJ_PROB System Code Table.
Procedure
Results
-
On the Consequence Modifier datasheet, the Consequence Probability that you deleted does not appear in the list of values in the Type box.
Note: The values in the existing Consequence Modifiers that have used the deleted Consequence Probability will not be affected when you delete the Consequence Probability.