Catalog Items
Queries Folder
The Catalog folder \\Public\Meridium\Modules\FMEA contains subfolders which contain baseline queries that are used by default in FMEA. The following table identifies the folder locations and results of these queries.
Query |
Behavior and Usage |
---|---|
Baseline queries for FMEA in folder \\Public\Meridium\Modules\FMEA | |
FMEA AnalysisTeam | Returns all team members for an analysis. The query is also used to support the FMEA Analysis TeamSub Report report. |
RCM FMEA Risks Without Recommendations Query | Returns the list of risks without any recommendations. |
Template List | Returns all FMEA templates of the selected template type. The query is used to support the Select Template window of the Apply Template Builder for FMEA. |
Baseline queries for FMEA in folder \\Public\Meridium\Modules\FMEA\Analysis | |
Criticality of RCM FMEA Assets | Returns number of RCM FMEA assets at very high, high, medium, and low criticality. |
FMEA Equipment By System | Returns select equipment records based on Analysis System ID. The query is also used to support the FMEA Analysis Description report. |
FMEA FailureModeEffects | Returns analysis details based on function, failure mode, and failure effects. This query is also used to support the FMEA Failure Mode Effects Analysis report. |
FMEA Overview Filter Query | Defines the parameters to be used to filter the FMEA Overview page. |
FMEA Recommendations by System | Returns recommendations based on the Analysis System ID. The query is also used to support the FMEA Recommendations report. |
Overview Page - FMEA Analyses | Returns all FMEA analyses for the Overview page list. |
Overview Page - Template | Returns all FMEA templates for the Overview page list. |
Graphs Folder
The Catalog folder \\Public\Meridium\Modules\FMEA contains the baseline graphs that are used by default in FMEA. The following table contains the graph names and details.
Graph |
Behavior and Usage |
---|---|
Percentage of Critical Assets with an Analysis | Displays a graph representing the percentages of critical assets that have an analysis. |
Percentage of Critical Assets an Analysis - LowMedium | Displays a graph representing the percentages of critical assets at low and medium that have an analysis. |
RCM FMEA Risks Without Recommendations | Displays a graph representing the number of risks without recommendations compared to the total number of risks. |
Reports Folder
The Catalog folder \\Public\Meridium\Modules\FMEA contains subfolders which contain baseline reports that are used by default in FMEA. The following table identifies the folder locations and descriptions of those reports.
Report |
Behavior and Usage |
---|---|
Baseline reports for FMEA in folder \\Public\Meridium\Modules\FMEA | |
FMEA AnalysisTeamSubReport |
SSRS report that is used by the FMEA Analysis Description report. |
Baseline reports for FMEA in folder \\Public\Meridium\Modules\FMEA\Analysis | |
FMEA Analysis Description | SSRS report that displays general information for an FMEA analysis, including the associated asset and team members. |
FMEA FailureModeEffectsAnalysis | SSRS report that displays detailed information of the FMEA analysis, including functions, failures, failure modes, and failure effects. |
FMEA Recommendations | SSRS report that displays detailed information of the FMEA recommendations for a system. |
Baseline reports for FMEA in folder \\Public\Meridium\Modules\FMEA\SSRS | |
FMEA Analysis Description | SSRS report that displays general information for an FMEA analysis, including the associated asset and team members. |
FMEA AnalysisTeamSubReport | SSRS report that is used by the FMEA Analysis Description report. |
FMEA FailureModeEffectsAnalysis | SSRS report that displays detailed information of the FMEA analysis, including functions, failures, failure modes, and failure effects. |
FMEA Recommendations | SSRS report that displays detailed information of the FMEA recommendations for a system. |
Dashboards Folder
The Catalog folder \\Public\Meridium\Modules\FMEA contains the baseline dashboard that is used for the FMEA Overview page. The following table contains the name of the dashboard and its usage.
Dashboard |
Behavior and Usage |
---|---|
FMEA Dashboard |
Displays the dashboard for the FMEA module, which contains the All RCM FMEA Risks Without Recommendations and Criticality Distribution of All Assets graphs. |